2023-04-18 12:56 AM
PART# STM32H747I-DISCO (Mouser S/O 935751)
We have a customer tried the demo program on ST website,
./en.STM32H747I-DISCO_demo/STM32H747I-DISCO_demo
"Three example programs based on TouchGFX�?STemWin�?EmbeddedWizard, open a random folder, use STM32CubeProgrammer write the hex file under Binary, then reset to run.
Onserve the screen, around 1s, the screen will blur, touch screen seemed fine. meanwhile if screen abnormal, no reponse if press reset button on board, power off and electrify again, display back to normal, but after a while the screen will show blurry again (the interval time is random). if we touch screen, the flash screen phoenomen will show up earlier."
Attached photos for your reference.
Could you advise how to solve it?
Solved! Go to Solution.
2023-07-12 7:25 AM
Hello LSong.11 ,
I receive the LCD daughterLCD DSI REV A09 MB1166 board and using this lcd , I tested each sub demo (TouchGFX , STemWin & EmbeddedWizard ) and they work correctly
2023-04-18 4:49 AM
Hello @LSong.1 ,
Thank you for bringing this issue to our attention.
I reported Internally.
Internal ticket number: 150025 (This is an internal tracking number and is not accessible or usable by customers).
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-28 9:04 AM
Hello @LSong.1 ,
Which STM32H747I-DISCO revision are you using? MB1248-H747I-D02, MB1248-H747I-D03 ...?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-28 9:10 AM
Hello @LSong.1
Setup:
Using STM32H747I- DISCO rev D03 MB12348 ,
Using LCD DSI REV A03 MB1166
Using STM32H747I -FW-V1.11.0 package
I test all the demo based on TouchGFX�?STemWin & EmbeddedWizard and it work correctly without any Screen Problem .
For LCD DSI REV A09 MB1166 that you are using for your board , I will order it to test ASAP to confirm & solve your issue ,I'll let you be informed as soon as I receive the LCD daughter board.
Thank you
Br
Moez
2023-05-05 1:38 AM
Hi @KDJEM.1 ,
is there any possible, the above problem is caused by the difference between MT25TL01GHBB and MT25QL512ABB. There're two different solutions about the QSPI flash on STM32H747I-DISCO.
2023-05-05 2:02 AM
or just caused by the corrupted spi flash
2023-07-12 7:25 AM
Hello LSong.11 ,
I receive the LCD daughterLCD DSI REV A09 MB1166 board and using this lcd , I tested each sub demo (TouchGFX , STemWin & EmbeddedWizard ) and they work correctly
2024-02-27 5:35 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.