cancel
Showing results for 
Search instead for 
Did you mean: 

Error: failed to download Segment[1] using STMcubeIDE v 1.14.0 & STMCube Programmer v 2.15

Anupurba
Associate II

I am trying to flash the STM32H753I-EVAL-2 board with a .hex file generated from STM cube IDE version 1.14.0. 
The code is build without error, but while loading it using the STMCube Programmer, I am getting the following errors:

Error: Failed to download Segment [1]

Anupurba_0-1705325908126.png

These are the options that I have selected while starting the programming : 

External Loader selected: M29W128GL_STM32H743I_EVAL

Anupurba_1-1705325986490.png

KIndly help.

 

11 REPLIES 11
Obdulia_FJones
Associate

@Anupurba how size is 2.33MB, it limit is 2MB available. U used external flash too?

thomas_joe
Associate

it depend on the file size

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.