cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H755 IWDG1 hardware watchdog in a continuous reboot and unable to recover the board

murali.karicheri
Associate III

I have a STM32H755 based board where we use M7 for BareMetal and M4 to run zephyr OS. We enabled IWDG1 in BareMetal and finds that the Flash erase of Bank 1 (M4 bank1, M7 bank 0) from Zephyr cause a reset and reset cause is IWDG1. Couldn't understand what is the dependency. M7 should be able run code from Bank 0 while erase happens on Bank 1.

Now I have enabled IWDG1 in hardware and the reload value is 5 msec. It continuously reboots and I am unable to connect the STMCubeIDE to halt the Cores from rebooting due to IWDG1. I have enabled Debugger0>Device Settings to have 'Suspend watchdog counters while halted "Enable", but IDE connects and disconnects immediately due to watchdog reboot which happens right away after boot. Is there a way to recover from this state.. Since I am not able to connect debugger or STMCube programmer, I am not able to flip the OB bit for hardware watchdog for IWDG1. Need help

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

You should be able to connect under reset, or boot into the bootloader by shorting BOOT0 to VDD during reset to connect and recover the device.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Super User

You should be able to connect under reset, or boot into the bootloader by shorting BOOT0 to VDD during reset to connect and recover the device.

If you feel a post has answered your question, please click "Accept as Solution".
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.