2025-12-18 12:19 AM
I am using a custom PCB design with a 480x800 pixel RGB input LCD display. I am driving the display via the LTDC peripheral. When I change the default colors, the color on the screen changes accordingly, which indicates that there is no apparent hardware issue with driving the LCD.
However, when I try to display a simple text on the screen using TouchGFX, the system enters the DMA2D_XferErrorCallback function due to a DMA2D error. Because of this, the text cannot be rendered on the display.
Could you please explain the possible reasons for this DMA2D transfer error and what might be causing it?
best regards
Celil Bayrakdar
Solved! Go to Solution.
2025-12-18 1:24 AM
Hello @celo01 ,
Which STM32 MCU do you use?
Does the issue happen also on other widget like an image widget or a texture mapper widget? I expect that if DMA2D_XferErrorCallback is entered when using texts, it will happen on all widgets using the hardware accelerator (check the list here). If my assumption is correct, you might have a issue with you hardware accelerator configuration.
2025-12-18 1:24 AM
Hello @celo01 ,
Which STM32 MCU do you use?
Does the issue happen also on other widget like an image widget or a texture mapper widget? I expect that if DMA2D_XferErrorCallback is entered when using texts, it will happen on all widgets using the hardware accelerator (check the list here). If my assumption is correct, you might have a issue with you hardware accelerator configuration.
2025-12-18 1:41 AM
merhaba
STM32H743GT kullanıyorum
2026-01-05 1:14 AM
Hello @celo01 ,
Could you confirm this?
@Osman SOYKURT wrote:
Does the issue happen also on other widget like an image widget or a texture mapper widget? I expect that if DMA2D_XferErrorCallback is entered when using texts, it will happen on all widgets using the hardware accelerator (check the list here). If my assumption is correct, you might have a issue with you hardware accelerator configuration.
2026-04-16 5:04 AM
Hello, I'm closing the thread due to inactivity. Feel free to open a new one if you still face the issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.