STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! touchgfx + STM32H7S78-DK

Hi,I am at the beginner/beginning stages trying to pick up STM32 ecosystem involving touchGFX and a display board STM32H7S78-DK. For now I would like to interact a touch button on screen to turn on an LED.Could I get guidance on the overall workflow ...

Text Glitching When in Portrait Mode

Hello,TouchGFX seems to have some sort of a “bug”, where in PORTRAIT orientation the text will glitch with some weird white lines, unless there is an image in the item-tree situated ABOVE text items. It doesn’t have to be any image in particular, but...

0fd253de-8d11-46a5-a67e-33b096e922a8.png Screenshot 2025-07-14 at 10.34.22.png a9b73ab8-47d8-41f0-a00c-7c03bf06f611.png 750f9146-1650-45b8-b89a-00c02c5ef565.png
montea by Associate II
  • 955 Views
  • 5 replies
  • 0 kudos

Resolved! DMA2D_XferErrorCallback function due to a DMA2D error

I am using a custom PCB design with a 480x800 pixel RGB input LCD display. I am driving the display via the LTDC peripheral. When I change the default colors, the color on the screen changes accordingly, which indicates that there is no apparent hard...

celo01 by Associate II
  • 671 Views
  • 4 replies
  • 0 kudos

TouchGFX Designer use high PC RAM

  Hi, Currently I face problem that TouchGFX 4.26.0 use a lot of PC RAM up to 9GB RAM Project info: Resolution 480x800Number of screen 26Number of custom container 82Support language: 5Typographies: 25 With the same design for resolution 272x480 ...

phatnt_0-1770092552241.png phatnt_1-1770092686202.png phatnt_2-1770092693403.png phatnt_3-1770092702924.png
phatnt by Associate
  • 329 Views
  • 2 replies
  • 0 kudos

TouchGFX 4.26.1 Designer Project Naming Issue

There have been great improvements to TouchGFX  Designer and the build process.  It now cleanly allows integration into the STM32CubeIDE project structure.  The problem is that even though you can provide a project name and the output will be placed ...

john-6 by Associate II
  • 341 Views
  • 2 replies
  • 0 kudos

Resolved! TouchGFX 4.26 Not rendering components correctly

Hi,I'm using TouchGFX to make a simple screen with just one slider. This to prove my graphics work and i can use touch to move the slider.I started with a CubeMX project this time but i got stuck somewhere.I enabled DMA2D and touchGFX.I see the DMA2D...

2026-02-24_16h17_08.png
SCous.1 by Associate II
  • 525 Views
  • 4 replies
  • 2 kudos

Resolved! CMD_LIST RAM size for STM32N6

Hi All,I'm currently developing a project using an STM32N655. I'm using a 1024x600 px screen. The image format is ARGB8888. Naturally, my frame buffer takes up approximately 2.5 MB. I needed to reduce the size of the CMD list.My application doesn't h...

Okeskin by Associate III
  • 601 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.