2021-04-13 6:19 PM
Dear TouchGFX Team,
I developed a display interface from TouchGFX 4.16 generated HAL and board configuration files that uses the following:
It is working very well, I have a swipe container that is smooth with no glitches. However there is an issue with the cover transitions. During the transition it does not hold the previous screen as the new one slides in, the area that should be the previous screen instead takes the GFXMMU default value.
Actually, when I run the code with a breakpoint on swapFrameBuffers(), only one of the buffers has the problem, the other one works fine. So during the cover transition the screen is swapping between a correct buffer(old screen in back with new one sliding in front), and the problem buffer(GFXMMU default value in back with new one sliding in front).
If I do single buffering the cover transition works properly (but the motion and the swipe container are glitchy due to the single buffer). I don't have enough ram space for an animation buffer, but from reading I don't think that cover transitions need one?
Any direction towards what might be causing this issue would be appreciated.
Thank you,
Russell
Solved! Go to Solution.
2021-04-14 6:13 AM
Hi,
The cover transition unfortunately does requires the animation buffer to work.
/Romain
2021-04-14 6:13 AM
Hi,
The cover transition unfortunately does requires the animation buffer to work.
/Romain
2021-04-14 6:16 AM
If you truly need one, what you could do is fake a cover transition where you slowly move your items to the left for example while having the ones from your other screen move in. Yu can also slowly fade them in and out. Once they are in place you then switch to the other screen (with no transitions since you have already the images/widgets where you want them to be).
/Romain
2021-04-14 10:00 AM
Thanks for the note.
Since it worked with single buffer without animation storage, and works correctly on one buffer in the dual buffer setup I was hopeful.
2021-04-14 10:08 AM
Try TouchGFX 4.13 target folder files
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.