2019-12-04 7:26 AM
In TouchGFX it is possible to call a C function when a flexi button is clicked (Trigger "touch") or released (Trigger "clicked").
Is it possible that the same button calls an "I_m_pressed()" function when you stay button clicked AND sends an "I_m_released()" as you release it?
Thanks a lot!
2019-12-05 12:21 AM
Hi,
I'm not 100% sure what you're asking, but - generally - you assign a handler to a button (A standard TouchGFX button - You could make your own with different arguments) and the event passed to that handler will tell you if it was a press or a release. There's no difference between a touch and a click.
ClickEventType is a part of the built in ClickEvent used for standard buttons classes.
typedef enum
{
PRESSED, ///< An enum constant representing the pressed option
RELEASED, ///< An enum constant representing the released option
CANCEL ///< An enum constant representing the cancel option
} ClickEventType;/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.