2023-05-21 4:28 PM
Whenever I add an image to project, even if not yet using it on a screen, I get the out of memory error upon trying to run the simulator. I remove the image and it compiles again.
Test image is only 88kB .png. Is this still too big? Had been compiling one day and not the next.
Thanks.
2023-05-24 8:51 AM
I realize I didn't provide much context. This is using TouchGFX Designer 4.21.4 on both Windows 10 and 11 machines. Turns out I can compile when I use a 32kB png image, but not an 88kB image. Is there simply a maximum image size requirement that I'm missing? When I run the TouchGFX Simulator I get the following error:
Run Simulator
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Reading ./application.config
Reading ./target.config
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Compile
make -f simulator/gcc/Makefile -j8
Reading ./application.config
Reading ./target.config
Compiling generated/images/src/image_RDM_TEXT_LOGO_-_black.cpp
cc1plus.exe: out of memory allocating 1073745919 bytes
make[2]: *** [build/MINGW32_NT-6.2/generated/images/src/image_RDM_TEXT_LOGO_-_black.o] Error 1
generated/simulator/gcc/Makefile:196: recipe for target 'build/MINGW32_NT-6.2/generated/images/src/image_RDM_TEXT_LOGO_-_black.o' failed
generated/simulator/gcc/Makefile:155: recipe for target 'generate_assets' failed
make[1]: *** [generate_assets] Error 2
simulator/gcc/Makefile:32: recipe for target 'all' failed
make: *** [all] Error 2
Failed
Failed
2023-05-24 12:02 PM
Hello. There should not be limits with image size this small, especially when your are running it with simulator. Have you test some other png picture same size, maybe there is something wrong with the image ? Can you share the image or simple project ?
2023-05-24 3:59 PM
I think you're onto something here @Jukka Pöppönen . I tried a downloaded 927kB image and no problem. Must be something wrong with the png files. Several company logo files have this same problem. Thoughts on figuring out what's wrong with the files?
2023-05-24 5:11 PM
2023-05-24 9:08 PM
Good morning. Even this picture is small in kilobytes, its resolution is huge 4859 x 1150. So the Cpp containing this image is 136 megabytes and thats too much. I got exactly same errors when test this image.
Guess its best to find image with smaller resolution or use some program to scale down resolution on this file.
2023-05-24 9:12 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.