2020-01-13 12:07 PM
2020-01-13 12:26 PM
Pretend it is an F407 without CRYPT/HASH
2020-01-14 12:48 AM
Thank you for the quick reply, unfortunately on the stm32F4 family product page I can see this:
STM32F407/417 – 168 MHz CPU/210 DMIPS, up to 1 Mbyte of Flash memory adding Ethernet MAC and camera interface
and seems that it doesn't have LCD TFT interface.
And also in TouchGFX on the templates I can't choose any of 417 or 407.
I'm I missing something here?
Can I add custom boards in TouchGFX?
2020-01-14 5:32 AM
The chip isn't designed to directly drive TFT displays, but can accommodate display controllers on the F(S)MC external bus. The F(S)MC could also support external memory for a frame buffer, but that would make for a very busy bus, and perhaps lack the bandwidth for a display.
Not familiar with the specific shield, but would assume it probably interfaces a display controller with integrated frame buffer.
I'd imagine custom displays could be supported, but would take work to develop drivers and integrate.
2020-01-16 5:54 AM
Thank you, i think FMC port is the solution for me, I watch some webinars about TouchGFX and now I see think better. I'll dive into FMC documentation. The display that I have is very popular and works with an ILI9486 interface which is pretty common and supported. After I manage to configure and make it work I'll post my experience here.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.