STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How to add programitacly item to ScrollWheel?

Hello,I want to show process history to user in my device. Max number of process is 30 but I will show last 5 process. There are two buttons (fill and empty ). If user press FillingButton first I will show filling image and filling text. if second ...

Epamuk by Associate III
  • 1052 Views
  • 1 replies
  • 0 kudos

Get an example TouchGFX

I wanted to use the example "Method 1 - From GUI task" TouchGFX. I downloaded PollDemoHwInt 4.9.3.zip. Unpacked. Can't open STM32CubeIDE 1.1.0?

AD�?b by Senior
  • 1076 Views
  • 4 replies
  • 0 kudos

Resolved! Processor Load calculation and (perhaps) display

The emWin demos show a processor load value on the screen, is there already a method defined for this in the TouchGFX / FreeRTOS configuration. I need to know how "near the edge" I currently am. It will help to know if I have enough processor HP to c...

Multiple Definitions Errors

I am getting compiling errors when trying to include a custom class into a TouchGFX project.I made a class called "test" with it's test.h and test.cpp components.//File: test.h   #pragma once class test { public: test(); ~test();   void s...

TLahr.1 by Associate III
  • 3255 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.