2020-01-17 12:08 AM
Hello ST,
I am facing Zoom in Issue of the Video.
I am using 480*272 display.
Please help me to fix this issue. I have searched whole datasheet , but nothing found regarding the resolution.
I have adjusted the DCMI crop settings also, please point me to the solution.
I have attached the images.
fig1: Expected video resolution displayed on TV
fig2: Present output screen on the 480*272 Display which is zoomed in.
I have even posted the same issue in the ADI site
https://ez.analog.com/video/f/q-a/121188/adv7180-camera-decoder-output-video-zoom-in-issue
Thanks,
Upender.
2020-01-17 3:20 AM
Hi @Uc.2361 ,
I'm using the ADV7182 and I would ask you about the data decoded.
I have DCMI configurated to External Synchronization, but the data received has the sync codes from ITU656 (linestart code (0x80), lineend (0x9d), framestart (0xAB) ...) so I needed to implement a decode code for this. It worked, but I spend a considerable resources from cpu to process this, when in fact the DCMI should do this. Indeed I have the YCbCr to RGB conversion by code too, so my frame rate is very low, about 4 frames/second.
Could you share/explain your DCMI setup?
Regards,
Anderson
2020-01-17 4:16 AM
Hello Anderson,
please find the DCMI configuration :
DCMI_HandleTypeDef *phdcmi;
phdcmi->Init.CaptureRate = DCMI_CR_ALTERNATE_2_FRAME ;
phdcmi->Init.HSPolarity = DCMI_HSPOLARITY_LOW;
phdcmi->Init.SynchroMode = DCMI_SYNCHRO_HARDWARE;
phdcmi->Init.VSPolarity = DCMI_VSPOLARITY_HIGH;
phdcmi->Init.ExtendedDataMode = DCMI_EXTEND_DATA_8B;
phdcmi->Init.PCKPolarity = DCMI_PCKPOLARITY_RISING;
phdcmi->Instance = DCMI;
Thanks,
Upender.
2020-01-17 4:39 AM
Hi Upender,
Well, the difference is only in the HSPolarity, I have HIGH polarity.
Do you get the raw camera data? Without the sync codes?
Do you use HAL_DCMI_FrameEventCallback() or HAL_DCMI_LineEventCallback() to trigger the camera data?
Thanks for reply,
Anderson
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.