2020-08-26 2:21 AM
I want to make a simple device to taking only photo and make decisions based on the photo. I would like to use the STM32WB as it has internal bluetooth modul. The camera module supports DCMI. The device will run on battery. After a few days of searching for info about STM32 and DCMI and I found info that only a few MCU supports DCMI interface :
STM32F2
STM32F4
STM32F7
STM32H7
STM32L4
The above info may be old, and the STM32WB familly is new.
So my question is, can I integrate the STM32WB and digital camera with DCMI interface to take a photo only.
Solved! Go to Solution.
2020-08-26 3:53 AM
Unfortunately there is no DCMI interface on the STM32WB.
2020-08-26 3:53 AM
Unfortunately there is no DCMI interface on the STM32WB.
2020-08-26 5:15 AM
We had an experiment with a very basic camera module connected via SPI to the WB. The frame rate was quite low even with a medium low resolution.
What are the possible interfaces available on your camera module? What is the expected picture resolution?
2020-08-26 6:21 AM
I have a raspberry digital camera, which is quite cheap. So I thought can use it.
The camera with SPI interface is more expensive. Could you please tell me the model of camera You used ?
2020-08-26 7:04 AM
The module we use is from ADAFRUIT and is name is ARDUCAMERA (like ARDUINO camera)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.