STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Add a field and its setter to a built-in class.

Hello!I have a swipe container with 3 pages in my TouchGFX app, running on an STM32F469 Discovery Kit. Everything is working fine, but I need to carry out certain actions when a swipe is started / ended. The docs state there are no built-in triggers ...

Update texts in a scrollist embedded in a scrolllist

Hello, I created a scrolllist where each item (container) contains a scrolllist with subitems (containers).Items and subitems have text areas which need to be updated. I know how to update texts in the items using "ScrolllistUpdateItem" in the Screen...

PDe N.1 by Associate
  • 1309 Views
  • 2 replies
  • 0 kudos

Persistent data

Hi,I am developing a small application on a STM32f746-disco, some parameters of which can be modified. I would like to store the modified parameters of this in memory in order to retrieve them on restart.As a maker beginner I am a bit confused on how...

Command line too long with GCC toolchain on Windows

I'm compiling the demo "TouchGFX Demo 2" (the one with the carousel: 2048 game, bird-eat-coin, home automation, ...).I also have a few peripherals/libraries in the project (freertos, mbedtls, lwip, fatfs, ...).This results in a large number of .o fil...

SZano by Associate III
  • 2407 Views
  • 2 replies
  • 0 kudos

Resolved! How to keep the last item of a scroll list keep at the bottom of list? (Not solved yet. When using setWindowSize, there are some error.. Please help me!! ) ==>Solved.

Dear TouchGFX team,After I made 6 items for a scroll list, I made them to show 3 items on a sreen.When I dragged to the top, the 1st, 2nd and 3rd item showed as I expected. And when I dragged to the bottom, I expected the last 3 items ( 4th, 5th and ...

JPark.14 by Associate III
  • 3649 Views
  • 5 replies
  • 0 kudos

BSP_LCD & GUI_ Functions cause HardFault

hello everyone,I'm getting this error; when I debug then launch the program, the GUI_ functions cause a hardfault, so I tried to change the main to start with the following (shown in the figure) with the BSP_LCD functions but I get same problem, how ...

0693W000002lC18QAE.png 0693W000002lBzCQAU.png 0693W000002lC0eQAE.png 0693W000002lC0yQAE.png
idrissmc by Associate III
  • 1856 Views
  • 3 replies
  • 0 kudos

Resolved! Can I and how to use STM32WB and the digital camera module with DCMI interface to take a photo only

I want to make a simple device to taking only photo and make decisions based on the photo. I would like to use the STM32WB as it has internal bluetooth modul. The camera module supports DCMI. The device will run on battery. After a few days of search...

PawelM by Associate III
  • 3166 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.