2026-04-13 7:29 AM - last edited on 2026-04-13 7:47 AM by Andrew Neil
Hello,
I have a STM32 NUCLEO-N657X0-Q development board. I wanted to interface with 8 digital PDM MEMs microphones.
In section 68.2 of the STM32N6 reference manual, it states that the N6 supports a "PDM interface, supporting up to 4 microphone pairs". Also in section 2.2.3 of AN5027, it states that if 8 microphone want to be used, the recommended data IO lines are SAI_D1, SAI_D2, SAI_D3, and SAI_D4.
Using CubeMX, I see no option for microphone pair 7-8. In addition to this, SAI_D4 doesn't exist when I search for the pin.
So how do I interface (if possible), the last microphone pair?
Thanks,
Christopher
Solved! Go to Solution.
2026-04-20 2:51 AM
Hello @csaji;
It is a typo, there are only three data IO: SAI_D1, SAI_D2, SAI_D3, in that case it will just support 3 pairs of microphones. Two microphones for each data line. So it supports actually 6 microphones.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-04-13 7:52 AM - edited 2026-04-13 8:02 AM
Hello @csaji and welcome to the community,
Thank you for bringing this issue to our attention.
I will report this issue internally for checking.
I will get back to you as soon as possible.
Internal ticket number CDM0061647(This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-04-20 2:51 AM
Hello @csaji;
It is a typo, there are only three data IO: SAI_D1, SAI_D2, SAI_D3, in that case it will just support 3 pairs of microphones. Two microphones for each data line. So it supports actually 6 microphones.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-04-21 4:00 AM - edited 2026-04-21 4:29 AM
See also: Connecting 8 PDM microphones to STM32N6
TL; DR: Datasheet DS14791 (Rev 9), AN5027 (Rev 2), and RM0486 (Rev 3) all have the typo.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.