2022-06-12 10:34 PM
I am interfacing 10bit OV camera with STM32F7508-DK to read the data from the camera. I want to upgrade to STM32H7 series, Is it camera example as per the STM32F7 DK is compatible with STM32H series Development kit.
Please let me know...
2022-06-14 6:39 AM
Hi @NS.9 ,
If you refer to this application note (AN5293), and precisely in section5 (table7), you can conclude that there is a compatibility for DCMI between the STM32F7 and STM32H7.
If your project is based on a generation of code with STM32CubeMX, this article can help you to migrate your current example to the STM32H7.
Another means, it is necessary to verify the compatibility of the camera module with the STM32H7.
Then, could you please precise the camera module you would like to use?
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.