2022-09-15 5:06 AM
If you choose the object "Static Graph"
and in this order:
set Y-axis Range Min = 60
set X-axis Range Min = 0
set X-axis Range Max = 8
click with the mouse into the Y-axis Range Min box
The value into the X-axis Range Max change itself at 60.0001 and is impossible to set again the correct value.
For us is a big problem.
Thanks Marco
2022-09-15 8:04 AM
The Great Carnac predicts a 4.20.1 release being issued soon. X-max is being compared against Y-min instead of X-min. That could cause a lot of problems. The fact that this has been undetected until now tells me how many people are actually using the static graph (at least in the Designer).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.