STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

stm32f429i-discovery dcmi->sdram address 0xD0000000

Posted on June 09, 2015 at 06:58Hello, I am working with stm32f429 using with a ov7670 camera with the dcmi using dma. It works fine if I do a capture into sram. I have also successfully initialized and tested the 8mb sdram @ 0xD0000000. What I wou...

prothan by Associate II
  • 2032 Views
  • 3 replies
  • 0 kudos

STM32F469 - Error in datasheet?

Posted on June 04, 2015 at 16:21Hello On page 18 of the http://www.st.com/st-web-ui/static/active/en/resource/technical/document/data_brief/DM00118914.pdfof the F469 MCU it is witten this about the DSI interface speed:Maximum speed per lane: 500Mbps...

Tantalum by Associate II
  • 1385 Views
  • 2 replies
  • 0 kudos

STM32F437 DCMI

Posted on May 07, 2015 at 17:43Hi ---I'm adapting working code from the STM32F407 Discovery platform to a custom board using the STM32F437. The process has been going well but I am having a problem with the DCMI. The control (I2C) channel works fine...

cmoses by Associate
  • 1245 Views
  • 2 replies
  • 0 kudos

SCCB emulation by I2C communication problem

Posted on May 13, 2015 at 01:17Hi,I have an application where I configure a OV7670 camera by SCCB bus (Omnivision thing) emulated by I2C...I used this sucessfully for couple of months but yesterday I disassembled the PCB that I have made for that ap...

Modal dialogs and pen up messages

Posted on April 13, 2015 at 23:39 I have a popup dialog that I load for some text entry. If I make it modal, the dialog procedure no longer gets 'pen up' events. If it is not modal, the user can interact with other things on the screen behind th...

hbarta2 by Associate III
  • 721 Views
  • 0 replies
  • 0 kudos

DCMI vs LTDC - simple Pinout on STM32F429 Discovery

Posted on March 31, 2015 at 20:32Hi! I have a simple yet hard problem. As is known, the STM32F429I discovery line has on board mainly ili9341 tft lcd. The job is to work with OV7670 camera through DCMI and with ili9341 through LTDC. But there is p...

sawingor by Associate II
  • 2826 Views
  • 5 replies
  • 0 kudos

STM32F417IGT6 FSMC A25 HardFault

Posted on April 12, 2015 at 11:16I have an ILI9325 TFT LCD connected to an F417IGT6 via FSMC Bank 1, Region 1, using 16-bits.The ILI9325 has an 8080-style interface, and FSMC A25 has been selected to drive register select as per AN2790 Figure 3 for ...

connect by Associate II
  • 2631 Views
  • 4 replies
  • 0 kudos

STM32F4 DCMI USB VCP

Posted on April 01, 2015 at 19:45Good  day, i'm new in using the *c STM32F4 i try to send data from DCMI to HOST(PC) via USB VCP but i nedd some help !! #stm-32f4-vcp-usb-dcmi

elbonay by Associate II
  • 1819 Views
  • 3 replies
  • 0 kudos

STM32 STemWin and Interrupt Problem

Posted on April 10, 2015 at 16:52 I'm using STM32F407ZGT6 with SSD1963 LCD controller and 800x480 TFT panel. I'm not using OS. It's working with STemWin.  But when I used any interrupt, code execution stops at somewhere in emWin.  I moved WM_Exec() ...

ilmete27 by Associate
  • 1318 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.