2015-05-12 4:17 PM
Hi,
I have an application where I configure a OV7670 camera by SCCB bus (Omnivision thing) emulated by I2C...I used this sucessfully for couple of months but yesterday I disassembled the PCB that I have made for that application and made some changes that arent related to the SCCB. After I put the PCB back with the kit the configuration that I have used for a few months stopped working...The function that I use is listed below...It gets stuck at while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED))...But the strangest thing that if I unplug the camera and connect all the pins through 20cm cable then the configuration works again. I found that out by testing if the module works at all. Simply if I add 20cm of cable (no pins were swapped) then it works again...I think it has something to do with the interference comming from DCMI but shouldnt the cables make it even worse?I have no rational explanation...Thanks very much for help...uint8_t SCCB_write_reg(uint8_t reg_addr, uint8_t* data){ uint32_t timeout = SCCB_TIMEOUT; // Send start bit I2C_GenerateSTART(I2C1, ENABLE); // Wait until I2C is busy while(!I2C_GetFlagStatus(I2C1, I2C_FLAG_SB)){ if ((timeout--) == 0) return 1; } while( !I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_MODE_SELECT)){ if ((timeout--) == 0) return 1; } // Send slave address (OV7670_WRITE_ADDR) I2C_Send7bitAddress(I2C1, OV7670_WRITE_ADDR, I2C_Direction_Transmitter); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)){ if ((timeout--) == 0) return 1; } // Send register address I2C_SendData(I2C1, reg_addr); while(!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_BYTE_TRANSMITTED)){ if ((timeout--) == 0) return 1; } // Send new register value I2C_SendData(I2C1, *data); while(!I2C_CheckEvent(I2C1,I2C_EVENT_MASTER_BYTE_TRANSMITTED)){ if ((timeout--) == 0) return 1; } // Send stop bit I2C_GenerateSTOP(I2C1, ENABLE); // Write done return 0;} #stm32 #i2c #dcmi #sccb2015-05-14 3:50 AM
Hi,
I dont know how is it possible but I found error in speed of the I2C bus at initialization. Basically one extra zero (from 100k to 1000k). I dont get how it got there or how it worked for few months if it was there all the time...Anyway the post above and this should work: // I2C config I2C_DeInit(I2C1); I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure.I2C_OwnAddress1 = 0x00; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_ClockSpeed = 100000; I2C_Init(I2C1,&I2C_InitStructure); I2C_Cmd(I2C1, ENABLE);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.