2015-12-21 8:37 AM
I have an STM32L152V8 running a large LCD using 1/4 bias and 1/4 duty. It works, but needs a little capacitive decoupling on the bias rails. I am using eternal decoupling pins PA0, PA2 and PA12, have enable external access to the bias signals with 'SYSCFG->PMC |= x0000000E' (LCD_CAPA) and have verified with my debugger that the register is indeed loaded with that value. I have also enabled those 3 pins as inputs per the manual.
The pins PB0, PB2 & PB12 are just floating, they should be .825, 1.65 and 2.45v. Apparently the pins are not being connected to the internal bias voltages. code: /*Configure GPIO pins : PB0 PB2 PB12, LCD_CAP pins */ __GPIOB_CLK_ENABLE() GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_2|GPIO_PIN_12; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); // CONFIGURE LCD bias voltages to pins PB0, PB2 & PB12 __SYSCFG_CLK_ENABLE(); SYSCFG->PMC |= 0x0000000E; Has anyone else used these pins? Thanks! #syscfg->pmc #lcd_capa #lcd-bias-voltage2016-01-05 11:44 AM
2016-01-05 12:07 PM
Is this an internal firmware bug?
Really not sure that's the right term here, the only software running is your own. You might want to look over the errata for chip related issues.This is primarily a user forum, as your question isn't getting any traction here, you might be better served contacting you local ST reps or FAE, and working it out through those channels.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.