STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Simulator peripheral window

I tried a search, but couldn't find the information. This is probably basic and simple, but I just couldn't find how to do it.I'm trying to bring up the Simulator peripheral window so I can emulate the key presses of the joystick in the STM32L4R9I-DI...

Du1 by Senior
  • 1386 Views
  • 3 replies
  • 0 kudos

Instance-agnostic APIs for screen transitions

I'm attempting to find a good way of providing a simple piece of inline code that can be executed to switch screen based on a third-party variable. The idea is to have one single event to trigger a screen switch, but letting the variable determine wh...

Resolved! Images are not correctly displayed

Hi I am using STM32F469 Disco Board. In TouchGFX Progress Indicator example the images gets blurred if i placed all the images in external nor flash. But if i placed the same images in internal flash, then it is working fine. What is the issue in...

PBU by Associate III
  • 1803 Views
  • 4 replies
  • 1 kudos

Cube MX template project + Error during code generation

Hi all,I'm starting with touch GFX on STM32F429 discovery, I find the firmware example, but I want to have the cubeMx template project for the STM32F429 discovery example ?Can ST share it ?the second issue that I'm facing is that sometimes when worki...

HasJen by Associate II
  • 3621 Views
  • 8 replies
  • 0 kudos

Selecting a LCD for a Commercial Project

I am interested in designing a product that has an LCD built into it. Up until now I have worked with the HMI type LCD's that you interface to by Serial with commands and now I am looking at actual LCD interface to make use of ST's GUI featureset (ht...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.