STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Touchgfx::BoxWithBorder constructor

Hi,I don't get why I can't set the border thickness/color directly when creating the BoxWithBorder object._boxWithBorder3(50, 50, touchgfx::Color::getColorFrom24BitRGB(150, 150, 250), touchgfx::Color::getColorFrom24BitRGB(0, 0, 0), 5,50)Indeed, it do...

GMeur by Senior II
  • 1468 Views
  • 2 replies
  • 0 kudos

STemWin Touch Driver (ADS7843) problem

Hello All,I am setting up STemWin on STM32F103VE MCU. The graphical part is all setup and working fine!The problem is the Builtin touch screen driver of STemWin. I have gone through the manual and created the low level SPI communication part and test...

0690X000008wKHsQAM.jpg

Resolved! How to create a blocking message box in touchGFX?

We have an existing embedded application with older GUI which is being ported to TGFX. For keeping the old logic, we want to display a blocking message box and wait for user response (button click) in a widget callback(GUI button callback). The probl...

zzzzz by Senior
  • 6770 Views
  • 14 replies
  • 0 kudos

STemWim is precompiled with wrong endianness ?

Hi, I am using STemWin on a ST32F429 in combination with a ST7735S connected to the cpu over an 8 bit interface. My pixel are 16 bit with color format RGB=565. My controller expects the bytes to be transferred R5G3, G3B5.The problem I am running into...

Resolved! I want to load a jpg image using touchgfx. I tried the JPEG_file_loader example but it doesn't compile either. Anybody can help me? Thanks

void Screen1View::setupScreen() { FILE* f = fopen("C:\\Temp\\image.jpg", "rb"); uint16_t width, height; JPEGFileLoader::getJPEGDimensions(f, width, height); BitmapId bmpId; //create dynamic bitmap matching file dimensions and in for...

Mvill.17 by Associate III
  • 1584 Views
  • 1 replies
  • 0 kudos

Resolved! setAction with an additional parameter

Hi,When using the 'setAction' function of the class Button, why can't I pass a callback object taking one more parameter than just the "const touchgfx::AbstractButtonContainer&"?Here's my CallBack object with its corresponding handler function:Callba...

GMeur by Senior II
  • 1218 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.