STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Error while linking project with TouchGFX and CubeMX

Hello!I try to create project with CubeMX 5.0.1 and TouchGFX Designer for Keil 5I have done all steps as written in this tutorial https://touchgfx.zendesk.com/hc/en-us/articles/360021620431-Configuring-STM32F429I-DISCOBut when I try to complie projec...

EEuge by Senior
  • 1701 Views
  • 6 replies
  • 0 kudos

STM32CubeIDE - Where is the STemWin library file?

I am starting a project from scratch using STM32CubeIDE (new STM32 Project), I select my 32F429Discovery board and select Initialize all periph to defaults.When the project opens in cubeMX, there is an error in the clock settings, and the graphics mi...

dave23 by Associate II
  • 1073 Views
  • 0 replies
  • 0 kudos

STM32F746 nucleo communication to LCD with FMC

I am setting new LCD screen with parallel 8080 protocol ( screen controller is SSD1351 ), I am using ST CubeMX to generate code for fmc ( attached picture of the configuration ). My problem is when I try to write command my D0-D7 is always 0 and my D...

davidra7 by Associate II
  • 1017 Views
  • 0 replies
  • 0 kudos

CAN bus and TouchGFX

Hi,In my system I have 2 devices connected over CAN bus (one on F746, second on F205), and F746 runs a TouchGFX application (800x600x16bpp) with 2 lightweight screens; FreeRTOS and SysTick configured to 100Hz. My problem is that image on screen may s...

0690X0000089Kx3QAE.png
itxs by Associate II
  • 4540 Views
  • 8 replies
  • 1 kudos

STM32CubeIDE and TouchGFX4.10 Starting New Project

Hi all,I tried to start a new project (from zero) in STM32CubeIDE with STM32F746DISCO board base, but I get errors in TouchGFX Generation Code when I Execute from CubeIDE, in the begginings...I could get working the new STM32CubeIDE and TouchGFX impo...

0690X000008w7OqQAI.jpg
eng23 by Senior
  • 2087 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.