STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! STM32F769I-DISCO Original hex file

Hello Everyone,I am testing the new Qt for MCU libraries on STM32F769I-DISCO. I should need of the original ST hex file flashed in STM32F769I-DISCO before shipment, I need it to do a fast comparation between Qt libraries and ST libraries.Is the a pla...

AlexGiov by Associate
  • 1836 Views
  • 2 replies
  • 1 kudos

Data signal for LCD (LTDC) not generated

Hi, Currently I'm programming STM32H743 for application which is using LCD TFT Controller. I'm using custom board. All RGB data signal not generated but other signal generated for example LCD clock signal, VSYNC, HSYNC. Anyone know how to solve?

ldanu by Associate II
  • 1117 Views
  • 1 replies
  • 0 kudos

Resolved! Custom LCD display has stripes on it

So i have gotten the LTDC working - sort of.I'm working off the app note 4861 which have an example on how to find the parameters for the display I'm using from datasheet.I'm using this display:https://www.buydisplay.com/default/low-cost-4-3-inch-480...

0690X000009k0V7QAI.png 0690X000009k0VHQAY.jpg
HP by Senior III
  • 1497 Views
  • 2 replies
  • 0 kudos

Using a CLUT with LTDC to reduce framebuffer size

Hello,I'm in the process of choosing a STM32 and determining whether an external SRAM/SDRAM is really needed for my application or not.The microcontroller will receive frames of pixels from a camera through SPI in L8 format (i.e 8bit grayscale images...

ikrosoft by Associate II
  • 3088 Views
  • 3 replies
  • 0 kudos

Incorrect color of standard buttons. png with transparent background. What is wrong?

Hi.The problem isThe project is in the memory of mcu (flash).button - OKThe project is in the memory of QUADSPI.what could be the problem?Добрый день.Проблема �?ледующа�?...Е�?ли пиши проект в mcu, отображает�?�? корректно. Е�?ли на флешку, то пропад...

0690X000009jsG9QAI.jpg 0690X000009jsGJQAY.jpg 0690X000009jsHCQAY.jpg 0690X000009jsHRQAY.jpg
lexabps by Associate II
  • 2720 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.