STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

DCMI interface doubles the image

Hello,I'm working on a DCMI to USB video class converter which runs on a STM32L496. The image sensor is a custom grayscale level sensor developed by my institution. It is 640x480, 8 bit per pixel, however to simplify the things I configured the DCMI ...

0690X000009jzWTQAY.png

Swipe Container selected page callback.

Hello,It would be nice to have a callback with selected page id from the Swipe Container. Now there is no way to know which page is selected. I need to know this because some constant (outside swipe container) widgets are depended from selected page....

Luk35 by Associate III
  • 2647 Views
  • 5 replies
  • 1 kudos

CubeIDE_1.0.2 Fatal errors When Building Project

Hello,I am trying to use a STM32F756 micro with the current CubeIDE and TouchGFX software. After setting up my micro in CUBEMX and generating code I attempt to build my project for debug but keep getting errors such as below:Description Resource Pa...

AGrif by Associate
  • 2006 Views
  • 3 replies
  • 0 kudos

Resolved! Is there any official library for graphs and scopes?

Hi,We will need to easily draw scientific graphs and scopes in our project, so I would like to know if there are or at least there are planned any libraries for TouchGFX to support this. Many advanced GUI design frameworks have such libraries but for...

Anguel by Senior
  • 1013 Views
  • 1 replies
  • 0 kudos

Resolved! Discard GestureEvent on Slider

Hi,I have a slider added on View. Also, my view overriders handleGestureEvent to handle it globally. Do you have any idea how to discard gesture event, when I quickly move slider?Same problem when My FrontendApplication overrides handleGestureEvent.

KMili by Associate III
  • 1372 Views
  • 2 replies
  • 0 kudos

CustomContainers with ClickListener

Hello,Why can't CustomContainers be created as 'ClickListener' objects?It's quite annoying as I'd like to create a ListLayout with clickable elements mainly through the studio and it seems the only way I can do it is through code as CustomContainers ...

GMeur by Senior II
  • 1029 Views
  • 3 replies
  • 0 kudos

Resolved! Scroll Wheel give error in custom container.

I am trying to design a custom container which has a scroll well. This scroll wheel item template has a wildcard. When I add a Scroll Wheel and generate code, compiler generates same variables three time in CustomContainerBase.hpp file. Like below;  ...

Resolved! Multiple calls to ...UpdateCenterItem when moving a scroll List, but last value of itemIndex is not the center item.

I've implemented a scroll list, following the documentation at https://touchgfx.zendesk.com/hc/en-us/sections/201785662-Tutorial-4-Creating-a-Scroll-Wheel-with-custom-behavior. Generally, it works. I have a function to update non-center items, and on...

RWebe.7 by Associate II
  • 1806 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.