STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! STM32F429ZE only has two options available (RGB666 and RGB565) in the LTDC configuration, there should be the RGB888 option according to the datasheet.

Hi, I'm not sure whether this is a bug in the Cube or whether I'm missing out something. I tried opening the F439 in the Cube and it has the 24-bit RGB option. Just to check while I was there I searched for the LTDC_B0 pin and found it on PE4, so I ...

CubeMX STM32H750B-DK

Hi,Another member of our team is working on hardware layout and is using CubeMX as a resource for configuring IO. They are having problems with CubeMX as it is not showing that you can load the STM32H750B-DK into the layout view. This would be helpfu...

belair55 by Associate III
  • 1151 Views
  • 1 replies
  • 0 kudos

TouchGFX Makefile doesn't seem to work in Linux?

I am trying to use the generated GCC make file (For target) in a Linux. I confirmed the project works when using it on windows through the TouchGFX.exe environment but it isn't wanting to cooperate in Linux? I am getting errors where if I run it as a...

Which QSPI flash would you choose for custom board?

I'm banging my head against this one. Initially I chose the W25Q128JV because it seemed like a suitable match for TouchGFX applications but it seems that the register layout is quite different from the (discontinued) Mircon part that is on the F746 b...

HP by Senior III
  • 6813 Views
  • 14 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.