STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Pre-rendered image scaling in TouchGFX designer

Is there feature to scale images in TouchGFX designer? I don't mean scaleable image widget that will be rendered on the MCU, I mean that the Designer tool can scale image and pre-render them to new size. Then all the heavy lifting of scaling is done ...

Tuoman by Senior II
  • 1540 Views
  • 2 replies
  • 1 kudos

Resolved! ST TouchGFX Demo source code

I want to try to make pattern password screen used in this video. Does this project have a accessible source code or document to get sample?https://youtu.be/FzBZeZQOG_k?t=183

Is DMA2D symmetric - read from display memory

The HAL hides so much functionality of the DMA2D IP block that I can't work this one out and the reference manual doesn't help much either!Writing a block of memory (e.g. bitmap file) to display memory window uses output offset to define the top left...

STM32CubieIDE - TouchGFX - STM32F469I-DISCO - Tutorial 2 -white noise on screen when adding an image.

I am working with the new CubeIDE and touchGFX. I try to do the Tutorial 2 (https://touchgfx.zendesk.com/hc/en-us/articles/205443722-Step-1-Setting-a-background-Image). Always when i insert the given images to my GUI, the screen on my board remains i...

Fab_0815 by Associate III
  • 1761 Views
  • 3 replies
  • 0 kudos

Error when creating applications

When I try to create a project for a Discovery Kit or open the online application in TouchGFX Designer, the "Downloading Application Template" and "Downloading GUI" slowly reach 100% and then this error screen is displayed:/*Sorry - something unexpec...

Henrik C by Associate II
  • 1026 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.