2019-10-15 3:34 AM
I want to implement Remote Display of TouchGFX screen through web server. Is this possible like VNC? How can I implement if possible?
Solved! Go to Solution.
2019-10-24 12:01 AM
You'd have to build your own interface for this - There's no such thing. I imagine this would be quite complex. You could translate the framebuffer into an image and send somwhere to be translated into a web page which should be reactive? Then you need to implement a complete TouchGFX interface for a web browser. Or, if it does not need to be reactive you could simply send the coordinates back through ethernet which would be easy to translate into a touchgfx click event.
2019-10-15 4:52 AM
Hi,
I'm pretty i've seen a VNC solution for stm32, generally, but it's not something i've tried. You could probably get it to run along side a TouchGFX application.
https://www.youtube.com/watch?v=XLjCwDoXHms
/Martin
2019-10-15 8:51 AM
there's some support for creating JPEG's I think - maybe that could be manhandled into sending MJPEG? Would be very interresting!
A starting point would be to create a new task to handle this and look into the image generation.
2019-10-23 9:09 PM
hi.
Thank you for your answer.
The posted URL works in the STemWin environment.
However, I do not want a VNC solution.
What I want is to build a web server on stm32f7 and view and control the screen of TouchGFX in a web browser.
This is because VNC has a constraint such as providing a dedicated program. I wonder if there is a possibility to control TouchGFX via web browser through iPad or iPhone without any setting.
2019-10-24 12:01 AM
You'd have to build your own interface for this - There's no such thing. I imagine this would be quite complex. You could translate the framebuffer into an image and send somwhere to be translated into a web page which should be reactive? Then you need to implement a complete TouchGFX interface for a web browser. Or, if it does not need to be reactive you could simply send the coordinates back through ethernet which would be easy to translate into a touchgfx click event.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.