STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Having STM32H743 issues on custom board. Will TouchGFX Application Template for STM32H743-EVAL be available soon?

I am setting up a custom board for the STM32F743 and only the first 18% or so of the screen is being displayed. The rest is garbage.. If I write directly to the framebuffer, the LTDC does write out to the display, so I know my SDRAM and LTDC are conf...

scottSD by Lead
  • 1192 Views
  • 1 replies
  • 0 kudos

Major problem with STMH743 version "V"

I've got a complex program running on the STM32H743 using LTDC to drive a VGA monitor, FMC for a SDRAM, and USB host to a keyboard. This works perfectly on the "Y" version of the chip.On the "V" chip it works but the LTDC output is less stable and th...

PMath.4 by Senior III
  • 3516 Views
  • 14 replies
  • 1 kudos

Resolved! How to show a picture?

Now I need to download a jpg/png/bmp picture to FLASH, and show it . I do not find touchgfx have anything with that. If I want to use touchgfx, how can I do?

Breeze1 by Associate III
  • 2927 Views
  • 6 replies
  • 0 kudos

Makefile path

Hello!I have created a new folder. It's called sensor. In this folder I put a .c and .h file.I also modified the Makefile this way:components := TouchGFX/gui target TouchGFX/generated/gui_generated sensorBut I get the following error:Compiling Core/S...

AVajd by Associate II
  • 7430 Views
  • 14 replies
  • 0 kudos

When I switch a working TouchGFX application from using LCD16bpp to LCD8bpp_ARGB2222 I get an Hard Fault when calling HAL::initialize()

I have a working F429 CubeIDE project that I want to switch from 16BPP to 8BPP, I changed:static LCD16bpp display; to static LCD8bpp_ARGB2222 display;and when I run the application I fall into Hard Fault when the application calls HAL::initialize().A...

MJPEG Example Problem

Hi,​Is there someone has the experience about MJPEG with AVI format?​I have try the CubeMX Source Code from STM32H743-EVAL, but it won`t work.I can display the First Frame and Second Frame, but after that it will keep showing this two Frame till the ...

emWin_PNG License issues

Hi,We have successfully integrated Segger's emWin_PNG library (https://www.segger.com/downloads/emwin/emWin_PNG) with STemWin on STM32H7 series MCU. Segger License agreement shown during emWin_PNG library download has below wording which might be an ...

STang.1 by Associate II
  • 888 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.