2020-03-12 10:39 AM
I am setting up a custom board for the STM32F743 and only the first 18% or so of the screen is being displayed. The rest is garbage..
If I write directly to the framebuffer, the LTDC does write out to the display, so I know my SDRAM and LTDC are configured and functioning properly.
I suspect a TouchGFX configuration issue and am wondering if the AT for the STM32H743-EVAL v3.0.0 will be available soon?
Solved! Go to Solution.
2020-03-12 11:49 AM
A bit of digging and I realized what my issue was with the configuration. When I set the Graphics Accelerator in the CubeMX TouchGFX Generator to "None" TouchGFX rendered the entire display.
While investigating this, I found that I had not enabled the DMA2D global interrupt.
After enabling that interrupt, and selecting the ChromArt Graphics Accelerator, TouchGFX correctly renders the entire display.
2020-03-12 11:49 AM
A bit of digging and I realized what my issue was with the configuration. When I set the Graphics Accelerator in the CubeMX TouchGFX Generator to "None" TouchGFX rendered the entire display.
While investigating this, I found that I had not enabled the DMA2D global interrupt.
After enabling that interrupt, and selecting the ChromArt Graphics Accelerator, TouchGFX correctly renders the entire display.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.