STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Problem with downloads to STM32F746G DISCO and TouchGFX demonstration program from FW F7 V1.16.0 repository

Hello, demo project is prepared for SW4ST32. After importing I can build all files without any problem.Then trying download (by Debug option from menu) I have achived some problems - but it seems that is flasded. On DISCO there is nothing until reset...

Set widget visible doesn't work properly

Hi,I have a problem when I want to make a widget visible.This code works :myStructure test; widget.setVisible(test.state); // test.state = bool widget.invalidate();But this code doesn't work :Container widget; myStructure test;   switch (index) { ...

MMerc.1 by Senior
  • 967 Views
  • 1 replies
  • 0 kudos

Touch Calibration

Hi,Following situation:I have a 480x272 display in portrait mode.(1) In TouchGFXDesigner the 0/0 point is top left with x-axis in horizontal and y-axis vertical down.(2) The expected (by the TouchGFX Framework) touch coordinates are 0/0 top right wit...

jimmii by Senior II
  • 3026 Views
  • 5 replies
  • 0 kudos

Is it worth using a TOUCHGFX display with STM32 ?

I need to know which interface I should use. It's for a display which is going to be used in hospitals. Have used other displays with other board as ESP32 for example connected through SPI.The question is, is it worth using a TOUCHGFX with STM32 if ...

JGonz.3 by Associate II
  • 3919 Views
  • 8 replies
  • 0 kudos

Resolved! Image takes up a lot of FLASH space

Hi,I want to use an image but it takes up a lot of space in FLASH memory when I add it.Example:Image size ------ (no image) ---- 7.55 KB -------- 2.38 KB (same picture but compressed)FLASH (free) ---- 811.97KB ----- 385.55 KB ----- 385.55 KB(Instead ...

MMerc.1 by Senior
  • 6910 Views
  • 15 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.