STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32F746g - syntax error: unterminated quoted string

I am trying to set up a simple project in STM32CubeIDE + TouchGFX and it returns me the following error: c: /st/stm32cubeide_1.1.0/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.make.win32_1.1.0.201910081157/ tools / bin / sh: syntax err...

JGonz.2 by Associate II
  • 8702 Views
  • 14 replies
  • 0 kudos

Can I drive a 4-lane mipi display with a STM32H7?

I'm thinking about using a high resolution display like this one​​https://www.ebay.com/itm/113385033095​But​ I read in the STM32H7 reference manual that it only has two mipi lanes, so my questionis if it is possible to drive a 4-lane display with onl...

m4l490n by Senior
  • 1118 Views
  • 0 replies
  • 0 kudos

Problem with background on Custom containers

When I have a custom container for a button which is the following. (Shown in order) TextAre - which is update able. Image - which is transparent in the middle under the Text. Background - dark background.When the custom contain for a button...

PSucr.1 by Associate II
  • 3716 Views
  • 7 replies
  • 0 kudos

STM32CubeIde TouchGFX and NT35510

Hello,i have a 4" Display with a NT35510 Controller from Waveshare. Their example works. Now I want to use the display with TouchGFX. Unfortunately I have no experience how to start. The Display is connected with FSMC. But in CubeMX i dont now, how S...

0693W000001cE9gQAE.png

How to use 6 bpp Color depth

Hello Martin,My project is using 8-color memory LCD, which only supports 3 BPP format. I found that touchgfx supports 6 BPP, which may simplify my code. But I found 24, 16, 8, 4, 2 and 1 bit options in touchgfx4.13. How to use the 6 BPP option? Thank...

hlian.1 by Associate II
  • 2834 Views
  • 7 replies
  • 0 kudos

Resolved! How to keep the same header bar for all screens?

I have requirements to keep a header bar with a number of status indicators visible on all screens. At first I created a custom component representing the header bar and placed it on all screens. But that is a duplication and any time I change screen...

PChil.1 by Associate II
  • 2109 Views
  • 2 replies
  • 0 kudos

STemWin5.44 lib missing GUI_SPLINE functions

Hello,Latest version of STemWin as included in STM32Cube_FW_L4_V1.14.0 apparently missing GUI_SPLINE_* functions in the provided *.a libs but they are listed in header file (GUI.h) - which causes linking error.We are working with STemWin_CM4_wc32_ot_...

APort by Associate III
  • 1100 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.