2020-05-14 10:29 PM
I'm thinking about using a high resolution display like this one
https://www.ebay.com/itm/113385033095
But I read in the STM32H7 reference manual that it only has two mipi lanes, so my questionis if it is possible to drive a 4-lane display with only 2 lanes, and if possible what would be the impact.
Also, is there a 720x1280 5.5", 6", 7", or 8" display with only two mipi lanes?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.