2019-11-25 1:05 AM
Hello,
Latest version of STemWin as included in STM32Cube_FW_L4_V1.14.0 apparently missing GUI_SPLINE_* functions in the provided *.a libs but they are listed in header file (GUI.h) - which causes linking error.
We are working with STemWin_CM4_wc32_ot_ARGB.a in particular but others are missing it as well.
This is very important feature for us.
Is there newer version, or version with this feature working?
Thanks in advance
2020-05-13 3:52 AM
Hej,
Could you solve this issue?
I´m using STM32Cube_FW_F4_V1.24.2. This results into the same issue. I´m also using the same lib STemWIN_CM4_OS_wc32_ot_ARGB.a.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.