STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

MVP TouchGFX

Could anyone suggest how to do...I have application with multiple screen, should be 200 or more.The model has pointer to active presenter. I have to know which interface the active presenter implements to call the methods. Do I have to try a dinamic ...

FMarr.2 by Associate III
  • 859 Views
  • 0 replies
  • 0 kudos

Animations only work well in one screen orientation

I’m running into an odd issue where animations work only in the “landscape�? orientation.Animations working fine:https://youtube.com/shorts/F-PeUQGEtPk?feature=shareWhen I change the orientation in TouchGFX and run the project again I get what looks ...

MBrus.2 by Associate
  • 981 Views
  • 1 replies
  • 0 kudos

How do I draw a line?

Hello everyoneHow do I draw a line using code. For example I receive over UART a number and I need to draw lines on my screen. Start and end positions are unknown also is the number of lines. until I know the user input So I need to draw a few lines...

Resolved! STM32429Eval Image Distortion

I am using Touchgfx v4.16. I recently purchased a STM32429I-Eval kit directly from ST. I ported an existing Touchgfx project to use the 429I-Eval drivers and flashed the board using the Stm32 Cube Programmer and the external flash loader that matc...

CPaye.1 by Associate III
  • 5558 Views
  • 6 replies
  • 0 kudos

TouchGFX Designer fails to generate assets

Hello,I have installed the following on my Windows 10 PC:STM32CubeIDE v1.6.0STM32CubeMX v6.2.0 STM32CubeProgrammer v2.6.0TouchGFX v4.16.1From the CubeIDE I can compile and debug code on my STM32F469I-DISCO board.However if I try to create an example ...

HGray.1 by Associate II
  • 2202 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.