2021-08-03 6:15 PM
I setup a radio button using my own image instead of one provided by TouchGFFX Designer. Initial size is say 24p. But then I realize it is too small, so I override the same image file name with an image of radio button but larger size say 36p. But the TouchGFXDesigner does not reflect the change although when run, the radio button size is correct e.g. 36p.
Why this is so? Is there any hard caching used by TouchGFX? I am using v 4.17.0
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.