STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Error to add a new Screen at touchgfx

Hello, I'm having a new problem with a touchGFX designer, when i try to add a new screen the CUBE IDE compiler generate many of erros.if i have 6 screens its okay, the CUBE IDE compile the code, but and i add the 7 screen, for some reason something h...

PCabr.1 by Associate II
  • 3420 Views
  • 0 replies
  • 0 kudos
DYann.1 by Senior II
  • 5992 Views
  • 19 replies
  • 1 kudos

Resolved! Screen refresh rate

Hello, The TouchGfx I used was version 4.15.0, and screen refresh rate​ is 60Hz. Now I move the project to version 4.17.0 TouchGfx, and the screen refresh rate is up to 70Hz. Can this parameter be changed by user?

V.H by Senior
  • 1050 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.