STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX hangs up at higher processor load

Hello!I have an STM32F777 with FreeRTOS and TouchGFX. An SPI display is controlled in partial framebuffer mode via SPI4 and DMA. The implementation is the same as in the TouchGFX demo projects with partial framebuffer (NUCLEO_C071RB + GFX01M2). I hav...

TouchGFX config.png TouchGFX_hang.png
Sandro_K by Associate III
  • 1937 Views
  • 9 replies
  • 0 kudos

Find index of first visible item in scrolllist

I am using a scrolllist that contains 6 items, 4 of which are visible. It is a horizontal list and non-circular. I'd like to have a couple of indicator items, one to the left and another to the right of the scrolllist to show whether there are items ...

GMeta.1 by Associate III
  • 679 Views
  • 1 replies
  • 0 kudos

Resolved! TouchGFX Demos

1.I have TouchGFX Designer 4.24.2 and STM32CubeMX running on Windows 11.  I downloaded the demos and examples via the file menu, also the latest TouchGFX Generator via CubeMX.  I am targetting a NUCLE0 STM32G071 with GFX01M2($AZ2) display, so I selec...

TJack.2 by Associate III
  • 1735 Views
  • 3 replies
  • 0 kudos

Resolved! TouchGFX build errors

I am using STM32CubeIDE 1.13.2 in Windows 11 and am trying to install TouchGFX.4.22.0 and its "Graphic Application" for a STM32H727i-DISCO board.The project is newly created and there are 14 errors that I need help fixing.As requested by the IDE, CRC...

TouchGFX image convertor

We are using TouchGFX for LCD UI design.  It seems that the generated c files for image have reverse-ordered 16-bit data.  We have to revert the image at run-time.  Is there a way to revert the 16-bit order during image converting?

lzlin by Associate
  • 575 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.