STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Hard Fault when performing a screen transition

Hello everyone,I'm currently developing a project using Touchgfx on a custom board with a STM32F469II and a 1024x600 screen on RGB565 format. I'm also using both an external SDRAM and Flash and the DMA2D is activated.Recently, I've been having an iss...

0693W00000Ho0wwQAB.png 0693W00000Ho17uQAB.png
TDele.1 by Associate III
  • 2168 Views
  • 1 replies
  • 0 kudos

Resolved! Change Clock Source STM32F429i discovery

Hello everyone!I'm working on a TouchGFX project on an STM32F429i discovery boardWhen creating project automatically, the default clock source selected in my project is HSE clock source with HCLK frequency of 168Mhz, the program works fine. But when ...

TTú.1 by Associate III
  • 2741 Views
  • 4 replies
  • 0 kudos

presenter pointer was NULL

Hi, The data read from Model class thru presenter in screen1View::screen1View() function was error. I debug the code and found the presenter pointer was NULL in constructor function. Is it unsafe to use at constructor and destructor function time ?

V.H by Senior
  • 1242 Views
  • 2 replies
  • 0 kudos

Resolved! Forbit clicks outside window

I need ModalWindow functionality where clicks outside it are forbidden. In my case my window is a container, how can I prevent clicks outside it?Seems easy but doesn't work for me. I tried make empty boxes and empty containers size of screen and set ...

VLau by Associate III
  • 1625 Views
  • 2 replies
  • 0 kudos

TouchGFX Flickering on STM32F746

Hi,I have a strange TFT flickering issue, and would love to hear your suggestions.The project running on STM32F746 chip, with SDRAM, and LTDC interface. UI is based on TouchGFX & FreeRTOS.Display is 1024X600 RGB (50 pin), based on HX8282 driverhttps:...

RZahor by Associate II
  • 4035 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.