STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Increasing Sensitivity to Swipes?

I'm working on a TouchGFX project for a 1.4" screen. The limited size means I'm taking all the space I can get, so widgets are commonly placed near the edges of the screen. If I have a swipe-able widget, such as a ScrollWheel, near the edges of the s...

TouchGFX with SPI TFT

I've created a simple project to interface a STM32L4R91-DISCO with a TFT using a SPI interface. I've attempted to follow the TouchGFX tutorial but thus far have been unsuccessful in getting the TouchGFX library to render anything.I have a task that s...

ebray by Associate II
  • 16924 Views
  • 31 replies
  • 0 kudos

The issue from importing STM32CubuIDE and TouchGFX

I tried many ways. However, the DAC 2 channel output is not active.The problem starts the commuity issue 'Undefined reference to 'HAL_RTC_Init' problem'​I tried the method you suggested, buf nothing displayed on the LCD.​So, I finished the integratio...

0693W00000JMxW1QAL.jpg 0693W00000JMxWkQAL.jpg 0693W00000JMxYMQA1.jpg 0693W00000JMxZAQA1.jpg
지한.1 by Associate II
  • 2026 Views
  • 2 replies
  • 0 kudos

Resolved! [Fixed Jan 24 2022] Issue connecting to Internet with TouchGFX Designer 4.16.1 and older

There is a current issue with TouchGFX Designer 4.13 to 4.16.1 where it cannot create a SSL/TLS secure channel, and therfor TouchGFX Designer cannot access the server and download projects and examples. We are currently investigating to fix this but ...

Resolved! CubeIDE not flashing external memory

Hello,I am working on a Project mainly from my desktop PC, yet because I recently installed my board in a garden shed, I have to use my Laptop from now on if I dont want to take the board home again. For this purpose I simply copied my projectfolder ...

0693W000008y4kAQAQ.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.