STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Hello I have a problem with my discovery bord "STM32F469I-DISCOVERY" when I use TouchGFX Designer and I only create a box (background) and a text area:

When I execute "run target" the compilation and flashing is successfully but I see nothing on the display of the board. When I do the same with simulator or with STM32CubeIDE everything is visible. The strange thing is when I add a button to my scre...

JHeyd.1 by Associate II
  • 1520 Views
  • 2 replies
  • 0 kudos

Resolved! Color corruption of text in TouchGFX 4.18.1

I created my project in TouchGfx 4.15.0. Currently I'm using TouchGfx 4.18.1. After flashing/debugging ; color of the text which I've given in TouchGfx is getting corrupted. For ex : If I set red(235 ,64 ,61) color to some text, after debugging it be...

LMath.2 by Associate II
  • 3369 Views
  • 7 replies
  • 0 kudos

Resolved! White screen after checking "Generate peripheral initialization as a pair of '.c/.h' files per peripheral" in CubeMX

I have an issue with TouchGFX on H750B-DK board.After I create a sample project in TouchGFX and import it into CubeIDE, I can then flash it to my board with no issues. But the project generated by TouchGFX is very messy (everything put into main.c), ...

0693W00000GZ6sSQAT.png
GHeller by Associate III
  • 2975 Views
  • 3 replies
  • 1 kudos

How to achive screen transition with swipe gesture?

I know it is possible to do a screen change with a button. But i would like to do it with swiping gesture. I defined transionits in FrontedApplication .cpp and .hpp files. The probelm is application crashes when transition is acalled:void MainScreenV...

0693W00000JNPE5QAP.png
manto.1 by Senior
  • 1876 Views
  • 3 replies
  • 0 kudos

Binary translations from external flash

The example in the help link below shows loading loading the translation from a file, but not from memory addressed external flash. This is what I'm using and mem_addr contains the expected data. The second argument to setTranslation() is a void poin...

Resolved! Why are European characters wrong in STemWin.

I opened and build a STM32F429 STemWin Hello world application in the latest STM32Cube Repository. All works fine, but if I add/change some European letters to the text, eg. Ä, Ö and Å are wrong. They are printed something like A+tilde and a "reverse...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.