STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Bug report: TouchGFX Designer 4.18.1 does not regenerate text source files properly if assets\texts\ is changed directly.

TouchGFX does not recognize if changes have been made into this file externally.Reproduce: make changes in assets\texts\texts.xml file -> regenerate with Designer -> texts/src/LanguageXXX.cpp source files are not regenerated properly.Fix: make change...

Tuoman by Senior II
  • 1018 Views
  • 1 replies
  • 0 kudos

Warning:"No internet connection" when starting TouchGFX-Designer. Although the other STM applications (Prg, MX etc) are working fine and get their updates via internet without any problem. The TouchGFXdesigner starts only without internet connection.

The corresponding Log-File reads: 2022-03-02 15:50:45,305 [11]ERROR Utils.WebHandling.WebHandler: The SSL connection could not be established, see inner exception.System.Net.WebException: The SSL connection could not be established, see inner excepti...

GWowe.1 by Associate II
  • 2170 Views
  • 3 replies
  • 0 kudos

Resolved! Problems with LCD screen disappearing?

The stm32f469 board is connected to the LCD of the MIPI interface.I made ScreenA, ScreenB using TouchGFX.(4.16.1)It operated ScreenA -> ScreenB -> ScreenA -> ScreenB every second.In the same program, sampleA put five images and sampleB put one pict...

PKunK.1 by Associate III
  • 7549 Views
  • 6 replies
  • 0 kudos

How to copy an image to RAM in TouchGFX?

We are working on the project using TouchGFX on the stm32f469 board.If you repeatedly display the screen made with TouchGFX as you proceed, the screen disappears. That doesn't mean the equipment stops. In debug terms, the timer is operating normally....

PKunK.1 by Associate III
  • 2951 Views
  • 4 replies
  • 0 kudos

Resolved! Tell me if TouchGFX has the ability to turn the screen

I worked with stm32f469i_Discovery.I worked with TouchGFX. LCD was working on 800*480, with icons and pictures.The LCD specification used has been changed. We need to use 480*800 longitudinal LCD.The previous work is 800*480, but I want to know that ...

PKunK.1 by Associate III
  • 2551 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.