2021-08-17 1:17 AM
TouchGFX is used for stm32f469i_Discovery.
I want to test External RAM because I can't express the picture well on the LCD screen.
I want to write 0xAF from 0xC0000000 to 0xCFFFFFFFF, and test if I read 0xAF when I read the same bungee, and I need advice on how to set up the program.
2021-08-18 9:20 PM
Hello PKunk.1,
I recommend you have a look at the example codes available in the STM32Cube F4 Firmware package (C:\Users\username\STM32Cube\Repository\STM32Cube_FW_F4_V1.26.0\Projects\STM32469I-Discovery).
To test you can comment the TouchGFX related functions in the main() function and perform some READ and WRITE after the RAM initialization is successful.
/Alexandre
2022-03-02 3:15 AM
Hi @Alexandre RENOUX ,
Can you please share me the ILI9806E code for initializing the ILI9806E module.
I can't change the LCD orientation . Currently set it as 480p width and 800p height. i wanna change it to 800 width and 480 height.
Thanks,
meimurgan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.