STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Compiling to Target issue with Callbacks

Code works fine in simulator but compilation to target (STM32756G-eval2).Code:// MainDisplayView.cpp   MainDisplayView::MainDisplayView(): viewCallback(this, &MainDisplayView::buttonNavCallbackHandler), boxClickedCallback1(this, &MainDisplay...

DMacD.1 by Associate II
  • 711 Views
  • 0 replies
  • 0 kudos

Critical bug: After update to 4.18.0 colors are incorrect on Hardware, but "Run Simulation" still works as expected

Here an example from the hardware  but in Run Simulation:We are using  touchgfx::TextAreaWithOneWildcardand the colors are wrong when we do not use 255,255,255 and 0,0,0. Only these two colors workWe use the following colors, and it is causing proble...

0693W00000GXAtzQAH.png 0693W00000GX9T9QAL.png 0693W00000GXAyLQAX.png
VSimu.1 by Associate III
  • 3227 Views
  • 8 replies
  • 1 kudos

Unable to write into LTDC registers

Hello everyone,I've been trying to integrate a simple TouchGFX project into STM32CubeIDE (so that I can add my own code to it), it's supposed to print simple graphics on the screen of a STM32L4R9I-EVAL board, but I stumbled upon an issue in the LDTC ...

Aksl by Associate III
  • 7548 Views
  • 15 replies
  • 0 kudos

Wondering if TouchGFX would be able to run on an STM32F411 with 512K flash & 128K of RAM. The screen I'd like to drive will take ~70K of RAM for a single display buffer.

I know there is no demo that runs on a 411. I'd also have to write my own display driver to transfer the display buffer. Just wondering if the 512K Flash and remaining 58K of RAM would be enough to fit TouchGFX and my own code in.

JimFouch by Associate III
  • 975 Views
  • 0 replies
  • 0 kudos

TouchGFX Designer 4.19 FlexButton bug

Hey @Martin KJELDSEN​ ,today I updated touchgfx in my project from version 4.18.1 to 4.19. As soon as I updated, regenerated and compiled my project I noticed that all of my wildcard texts in flexbuttons are missing:Example code:#include <gui/screen1...

0693W00000KdgusQAB.png 0693W00000Kdgv2QAB.png 0693W00000KdgyBQAR.png 0693W00000Kdh07QAB.png
JureL by Senior
  • 1260 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.