STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

DSI Video Mode on STM32L4R9AI-EVAL using GFXMMU_Lut

I have successfully adapted a 480x480 round LCD to attach to the STM32L4R9AI-EVAL kit and can display an RGB888 image continuously, with a custom GFXMMU_Lut that reduces the required frame buffer to 558,336 bytes, and the frame buffer located in SRAM...

rgree.1 by Associate II
  • 2082 Views
  • 3 replies
  • 0 kudos

UART HAL Timebase matters?

I am running FreeRTOS on an STM32H745I board in a TouchGFX application. All tasks I want to run are on the M7 core. I'm trying to periodically send data over UART3 to the virtual COM Port of the STLink. The HAL returns an ok status when transmitting,...

EMurp.1 by Associate II
  • 2863 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.