STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Replicate touchgfx based-project on a web server

Hi guys, many customers ask for a web page that looks the same as the display on the machine, developed on touchgfx with STM32 microcontrollers.The goal is to control the screen also from the web page.Is there a way to do that? Maybe with an LWIP web...

EA.1 by Associate
  • 1548 Views
  • 2 replies
  • 0 kudos

STM32L4R9I-EVAL : How to select the MB1315 screen ?

Hello everyone !I'm using an STM32L4R9I-EVAL board to work on a GUI with TouchGFX and I want to use the MB1315A rectangular screen, and not the MB1314 (little round screen) because it better fits my needs.So I created a dummy project with TouchGFX (i...

Aksl by Associate III
  • 2679 Views
  • 2 replies
  • 1 kudos

How can I use color keying in STM32H7?

I want to make the specific color of the image transparent.This is different from the alpha of the entire image.There is a method that can be used for 16p of the Color keying document, and I want to know the detailed usage and code.Can I get a sample...

Resolved! STM32H735G-DK's DMA2D Start Address Drifts

I'm using CubeMX to generate the start file rather than the BSP example. When I tried to set the DMA2D, I found that the start address will be shifted by 0xC.... // setup octospi2 for hyperram, dma2d and ltdc above uint32_t col; uint32_t startAdd = 0...

GChen.5 by Associate II
  • 2174 Views
  • 2 replies
  • 0 kudos

X-CUBE-TOUCHGFX 4.18.1 is out

TouchGFX 4.18.1 is now online.Release notes (which can be found in the online documentation) are as follows:Bugfixes in TouchGFX Designer:Various network stability fixesAdding images to a project that contains a Progress Indicator while TouchGFX Desi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.