STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

how can i convert image.png color with BmpCvt.exe to an buffer 8 bit like stlogo.h and plot it in stm32f796i-discovery with a function BSP_LCD_DrawBitmap(uint32_t Xpos, uint32_t Ypos, uint8_t *pbmp) ??

i convert an image RGB to a buffer 8 bits and plot it with a function BSP_LCD_DrawBitmap(), but not work correctly like logo image.please any idea ?thank you.

Abdou by Associate II
  • 3494 Views
  • 2 replies
  • 0 kudos

i cant get RAW imagenes in stmf429

Hi everyone I,m having a problem when i try to capture a photo in raw format with the OV5640 camera. I get an image of a suitable size but it adds the header of the JPEG that i want to avoid it.When i try to open it with the image viewer, i can see ...

EGord.2 by Associate
  • 1155 Views
  • 1 replies
  • 1 kudos

Regenerate code with TouchGFXDesigner

I am trying to get familiar with the workflow for using TouchGFXDesigner with CubeIDE, when I create a project with the designer and import it to the CubeIDE all works fine, but for example I change the name of a screen in the designer and regenerate...

JVALL.1 by Associate III
  • 3098 Views
  • 5 replies
  • 0 kudos

Debug touchGFX project from external QSPI in EWARM

Hello,Working on touchGFX project (ide: IAR workbench 8.40) for STM32H750B-DK board and its working (generate code, run simulator, run target from TouchGFX generator tool) as well as successfully build in IAR also. But I couldn't debug this project f...

RLalj.1 by Associate II
  • 1822 Views
  • 2 replies
  • 0 kudos

New TouchGFX text doesn't show up in IAR

We have been having this issue for a while. We are in TouchGFX version 4.19.1 (but it seems to be an issue in most versions). For a while we were able to add text in touchgfx and everything worked great. Then after a while TouchGFX wouldn't create...

RPett.2 by Associate II
  • 4353 Views
  • 8 replies
  • 0 kudos

Resolved! External RAM Problem

Hi Everyone,I am working on a project with TouchGFX. I'm working with STM32H743X MCU. Project have MT48LC4M32B model external SDRAM. I was have an issue with screen that corrupted image on it. You can see below some example at picture.In expectation,...

0693W00000Nrqh7QAB.jpg 0693W00000NrqmAQAR.png 0693W00000NrqmFQAR.png 0693W00000NrqmPQAR.png

Resolved! Problem with TouchGFX on STM32H747-DISCO: freezing while an other task runing with higher priority.

Hi ! I'm currently working on a STM32H747-DISCO with TouchGFX to test and discover this graphic library. My touchGFX app is only 2 screens with a button to go screen 1 or 2 with a slide animation.But when I'm implementing an other task in FreeRTOS wi...

LBESO.1 by Associate III
  • 11712 Views
  • 25 replies
  • 0 kudos

Resolved! Rotate text at any angle

Currently it seems that text can only be rotated by a multiple of 90 °. In a current project, however, I have a customer requirement that text must be rotated by any angle, since the display must be mounted rotated. What would be the best approach to...

UVett.1 by Associate II
  • 5693 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.