STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

lcd_i2c_setCursor function for LCD 20x04

I hope this is the right section of the site to ask this question, otherwise please redirect this thread.I just started programming, I am using a 20x04 LCD with stm32F407G and I need the classic function " lcd_i2c_setCursor (row, col); ". I am not ab...

luke514 by Senior
  • 11296 Views
  • 2 replies
  • 0 kudos

How can I have several external sections?

Hi dearsHow can I have several external sections in cuneIDE?and how can learn to touchGFX that separates Images?for example, 3 images place in ExtSection1 and the rest in ExtSection2.  here we have only two sections.

0693W00000Y7V5lQAF.png 0693W00000Y7V7IQAV.png
MTora.1 by Associate III
  • 2300 Views
  • 7 replies
  • 0 kudos

Where is a GFX screen stored?

Happy New Year to you all.A little help please...I may have been a little ambitious with this project, but here goes.I have made a board using a STMf429igt (176 pin).This is based on the STM32F429 Eval board, (which uses the BGA216 version of the pro...

derek2399 by Associate II
  • 3306 Views
  • 6 replies
  • 0 kudos

Resolved! Number display issue

ToughGFX Designer: 4.20.0STM32Cube IDE: 1.11.0Hello there,i'm using touchgfx to show received data usingUnicode::snprintf(FenceNumBuffer, FENCENUM_SIZE, "%d", g_displayCtlBlk.fenceConfigS1);Recently I found if I place FenceNum.resizeToCurrentText();d...

JPan.4 by Associate III
  • 2546 Views
  • 4 replies
  • 0 kudos

How to access or reference a variable set in a custom container from the screen containing that container

I have a custom container that pops up on a screen for password entry. The password is set using 4 scroll wheels and an entry button with icon. When the entered password matches the required password a flag variable is set and the custom container is...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.