STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Background corrupted during transition

I am having an issue with transitions between screens. I’m using a cover transition but as soon as the transition starts the background turns to noise however the new screen covers it gradually as expected. The program is running from QSPI flash on a...

0693W00000BdbZtQAJ.jpg
CPink.1 by Associate
  • 3790 Views
  • 5 replies
  • 1 kudos

Resolved! Issue with importing translations into TouchGFX!!!

I sucessfuly exported texts.xml with translations.rbbut when I try to import .xlsx back to .xml. I get the error sheet Typography not found!?> translations.rb import texts.xlsx texts.xml   sheet 'Typography' not found   An error occurred during trans...

manto.1 by Senior
  • 5804 Views
  • 8 replies
  • 0 kudos

TouchGFX, STM32H7 compatibility

Is it possible to use TouchGFX to visualize an FFT algorithm from the Nucleo STM32H7A3 144 board? Im new and dont know if its possible to connect a GUI from this board to a monitor via TouchGFX.Thanks

ZShep.1 by Associate
  • 1443 Views
  • 2 replies
  • 0 kudos

Resolved! Hardware Button

Hello, I have been trying for 2 days to read my hardware button from the STM32F746G board and change the color on the display. Unfortunately, all tutorials are for older versions where the file ButtonController.hpp still exists, but in TouchGFX 4.21....

AGeis.4 by Associate III
  • 2990 Views
  • 4 replies
  • 0 kudos

Frequently loading a Dynamic Graph or Static Graph will freeze TouchGFX's screen and render it inoperable.

Frequently entering and exiting a screen with Graph in it, touchgfx will end up frozen on image2's screen and not fully loaded into image1's state.Program run process: xxxScreenViewbase::xxxScreenViewbase ---> xxxScreenView::xxxScreenView ---> xxxScr...

0693W00000Y9nyJQAR.png 0693W00000Y9nynQAB.png

why the interface of STM32F769I DISCO KIT generated by TouchGFX is Freezing even for a very simple button test?

to more explainI installed TouchGFX 4.20.0, I developed a simple interface that has two buttons just for a very simple test, I sent this program to the STM32F769I DISCOVERY KIT board, everything goes well, I received the message Run Target DONE, the ...

RMOHA.21 by Associate
  • 1081 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.