STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Sending an I2C command using TouchGFX UI

Board: STM32F429I-disco1How can I send an I2C command when a button is being pressed? So I set up a FlexButton to act as a toggle button and set its interaction to call a function (ToggleMute) which I would need to implement.My idea was just to use t...

MexiAxel by Associate II
  • 1863 Views
  • 1 replies
  • 1 kudos

Video mode printing another frame on screen

Using STM32F469I-DISCO in video mode, the testing screen created in TouchGFX Designer is being printed to the DISCO board in video mode. The issue I am encountering is the start of the frame is being printed again and I am not sure how to solve this ...

touchgfx_designer.png otm8009a_video_mode.png
JSime.1 by Associate II
  • 2231 Views
  • 2 replies
  • 0 kudos

Resolved! TouchGFX Scroll Wheel Selected Element during animation

Hi allI want to create a GUI, similar the Scroll Wheel in the provided examples.The only difference to the Example i need, is that it should always update the Selected value from the scroll wheel. Also when moving around. So I used the scrollWheel.ge...

MMess1_1-1697119512545.png
MMess.1 by Associate III
  • 2438 Views
  • 1 replies
  • 0 kudos

Resolved! white screen on custom GFX01M2 board

I made a custom STM32 board based on the schematics of Nucleo-G071RB and X-Nucleo-GFX01M2. On the development board, the TFT LCD works. However, when I program my custom board using STLINK-V3SET, the TFT LCD only shows a white screen.I did changing T...

Dev_P0_1-1697602980764.png Dev_P0_2-1697603069000.png
Dev_P0 by Associate
  • 1494 Views
  • 1 replies
  • 1 kudos

TouchGFX - Serial Wire debug problem

Hi. I'm using  the STM32F469 Discovery kit (32F469IDISCOVERY) and the code generated with TouchGFX Designer (4.21.3) works fine (showing GUI on the screen) until I set "Debug: Serial Wire" using CubeMX. Then the screen remains black. The strange thin...

PWojd by Associate
  • 2608 Views
  • 3 replies
  • 0 kudos

Resolved! how to get model instance?

Hi.What I want is call model function(C++ function) in C.I dont use rtos.I add simple Queue in model and in tick function, check queue, pop and to do something.in queue just push one data (type int)I want to push Queue in model in C, but I dont know ...

hben by Associate
  • 1294 Views
  • 1 replies
  • 0 kudos

Resolved! DCMI DMA interrupt on STM32F746 disco board

I'm currently working with the STM32F736 Discovery board and an OV5640 sensor. I've successfully configured the DCMI for snapshot mode and enabled DCMI DMA interrupts. However, I've encountered an unusual issue. While I observe that the capture bit c...

Compilation Errors: Not Declared In Scope

Good day I am trying to interface my GUI on my STM32F429i-DISC1 board for my final-year project using STM32CubeIDE (1.6.1) and TouchGFX (4.16.0 - 4.17.0 won't run on my PC so I opted for an older version) and I have run into the following problems (s...

LNdungane by Associate II
  • 2061 Views
  • 1 replies
  • 0 kudos

Resolved! Display buffer color formats in TouchGFX

I’ve already asked and didn’t get any answer to the following question: how did it happen that TouchGFX, being ST product, does not support the very basic HW feature of each and every LTDC interface in STM32 controllers, namely – L8 (8bpp) format wit...

bear2023R by Associate III
  • 4020 Views
  • 6 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.