2023-10-17 9:40 PM
I made a custom STM32 board based on the schematics of Nucleo-G071RB and X-Nucleo-GFX01M2. On the development board, the TFT LCD works. However, when I program my custom board using STLINK-V3SET, the TFT LCD only shows a white screen.
I did changing TFT LCD(DT022CTFT) : new TFT LCD just same.
this is my custom board's MCU.
This is my custom board's SWD pins
1. How can I program using STLINK-V3SET in TouchGFXDesigner?
Solved! Go to Solution.
2023-10-24 2:59 AM
oh.... I forgot DISP-NRESET is not PA1 in my circuit. (X-NUCLEO-GFX01M2's DISP-NRESET is PA1)
I change DISP-NRESET pin to PA4, and working fine
2023-10-24 2:59 AM
oh.... I forgot DISP-NRESET is not PA1 in my circuit. (X-NUCLEO-GFX01M2's DISP-NRESET is PA1)
I change DISP-NRESET pin to PA4, and working fine
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.